Incremental Display Support on Vybrid MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Incremental Display Support on Vybrid MQX

跳至解决方案
1,134 次查看
ioseph_martinez
NXP Employee
NXP Employee

Hello,

Is this the right forum to ask for new requests to MQX? Please let me know.

I have a customer asking for a flexible way to add more displays into the BSP. Currently 2 steps are required to add an extra display:

-Add a desired configuration _dcu4_default_timings[]
-Modify BSP init_dcu4.c config values: _bsp_dcu0_init to the desired resolution

And you need to rebuild the whole BSP.

That is quite time consuming. Could not be a mechanism to dynamically add new supported displays? (key challenge is the display is initialized during bsp init, somehow it should be possible to re initialize the driver on a task with a new configuration perhaps during runtime)

If there is a way that it can be done that would be great.

Thanks,

Ioseph

标记 (3)
0 项奖励
回复
1 解答
977 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

There is  a public community for MXQ: MQX Software Solutions

在原帖中查看解决方案

0 项奖励
回复
2 回复数
977 次查看
naoumgitnik
Senior Contributor V

Hello Ioseph,

If this request is not really related to Vybrid but rather generic, I would not expect that much reaction to it...

Do we not have a dedicated MQX Community space?

Regards, Naoum Gitnik.

0 项奖励
回复
978 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

There is  a public community for MXQ: MQX Software Solutions

0 项奖励
回复