Incremental Display Support on Vybrid MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Incremental Display Support on Vybrid MQX

ソリューションへジャンプ
1,189件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Hello,

Is this the right forum to ask for new requests to MQX? Please let me know.

I have a customer asking for a flexible way to add more displays into the BSP. Currently 2 steps are required to add an extra display:

-Add a desired configuration _dcu4_default_timings[]
-Modify BSP init_dcu4.c config values: _bsp_dcu0_init to the desired resolution

And you need to rebuild the whole BSP.

That is quite time consuming. Could not be a mechanism to dynamically add new supported displays? (key challenge is the display is initialized during bsp init, somehow it should be possible to re initialize the driver on a task with a new configuration perhaps during runtime)

If there is a way that it can be done that would be great.

Thanks,

Ioseph

タグ(3)
0 件の賞賛
返信
1 解決策
1,032件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

There is  a public community for MXQ: MQX Software Solutions

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,032件の閲覧回数
naoumgitnik
Senior Contributor V

Hello Ioseph,

If this request is not really related to Vybrid but rather generic, I would not expect that much reaction to it...

Do we not have a dedicated MQX Community space?

Regards, Naoum Gitnik.

0 件の賞賛
返信
1,033件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

There is  a public community for MXQ: MQX Software Solutions

0 件の賞賛
返信