Hello,
Is this the right forum to ask for new requests to MQX? Please let me know.
I have a customer asking for a flexible way to add more displays into the BSP. Currently 2 steps are required to add an extra display:
- | Add a desired configuration _dcu4_default_timings[] |
- | Modify BSP init_dcu4.c config values: _bsp_dcu0_init to the desired resolution |
And you need to rebuild the whole BSP.
That is quite time consuming. Could not be a mechanism to dynamically add new supported displays? (key challenge is the display is initialized during bsp init, somehow it should be possible to re initialize the driver on a task with a new configuration perhaps during runtime)
If there is a way that it can be done that would be great.
Thanks,
Ioseph
Solved! Go to Solution.
Hello Ioseph,
If this request is not really related to Vybrid but rather generic, I would not expect that much reaction to it...
Do we not have a dedicated MQX Community space?
Regards, Naoum Gitnik.