Increase DATA SIZE in MQX project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Increase DATA SIZE in MQX project

1,809 次查看
Nouchi
Senior Contributor II

Hello,

My MQX application (M4 side) needs now more ram.

Code is located in SysRAM0 (0x3f000000) with 256kB, and TCMU seems to be only 32kB.

I would to allocate 192kB (0x3f000000 - 0x3f02ffff) for the code and 64kB ( 0x3f030000 - 0x3f03ffff) for data.

It seems data can't be accessed on SysRAM0.

How to share with llinux (A5 side) small amount (64 or 128kB) of DDR ?

Regards,

Emmanuel

0 项奖励
回复
2 回复数

1,594 次查看
Carlos_Musich
NXP Employee
NXP Employee

You can also access 0x3F04_0000

pastedImage_1.png

This is shared RAM as you can see in the linker file:

define exported symbol __SHARED_RAM_START               = 0x3f040000;
define exported symbol __SHARED_RAM_END                 = 0x3f04fff0;

the linker files are located in next paths:

C:\Freescale\Freescale_MQX_4_2\mqx\source\bsp\twrvf65gs10_m4\iar

C:\Freescale\Freescale_MQX_4_2\mqx\source\bsp\twrvf65gs10_a5\iar


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,594 次查看
Nouchi
Senior Contributor II

Hello  Carlos,

SysRAM1 seems to be already used for libmcc exchanges, in fact I would like to increase data memory heap.

Where should I move DATA_BASE_ADDR_START segment to have more than 32kB heap memory?

ram.scf  (for DS-5)

#! armcc -E --cpu Cortex-M4

#define CODE_BASE_ADDR_START    0x3f000000                ; SysRAM0
#define CODE_BASE_ADDR_END      0x3f03fff0
#define CODE_SIZE               (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START)

#define DATA_BASE_ADDR_START    0x3f800000                ; CM4 TCMU
#define DATA_BASE_ADDR_END      0x3f807ff0
#define DATA_SIZE               (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START)

#define DATA_SHARED_START       0x3f040000
#define DATA_SHARED_END         0x3f04fff0

#define TCML_END                0x1f807ff0

;
; Note:
;   memory range 0x3f07ebf0 - 0x3f07eff0 is reserved for bootloader_vybrid segment
;
#define MY_ALIGN(address, alignment) ((address + (alignment-1)) AND ~(alignment-1))


LOAD_REGION_INTRAM CODE_BASE_ADDR_START
{
    VECTORS CODE_BASE_ADDR_START
    {
        vectors.o (.vectors_rom,+FIRST)
        vectors.o (.cfmconfig)
    }
    
    CODE +0
    {
        * (InRoot$$Sections)      ; All library sections for example, __main.o,
                                  ; __scatter*.o, __dc*.o, and * Region$$Table
        * (KERNEL)
        * (.text)
        * (+RO)
    }
    
    RAM_VECTORS DATA_BASE_ADDR_START ; For ram vector table. Used when  MQX_ROM_VECTORS is set to zero.
    {
        vectors.o (.vectors_ram)
    }
    
    DATA +0 ALIGN 32
    {
        * (+RW, +ZI)
    }

    KERNEL_DATA_START +0 ALIGN 16
    {
        * (KERNEL_DATA_START)     ; start of kernel data
        * (SRAM_POOL_START)
        * (UNCACHED_DATA_START)
    }

    KERNEL_DATA_END DATA_BASE_ADDR_END - (0x03*0x10)      ; RAM_END - 3 x aligned value with align 0x04
    {
        * (SRAM_POOL_END)
        * (UNCACHED_DATA_END)
        * (KERNEL_DATA_END)     ; end of kernel data
    }
 
    SHARED_RAM_START DATA_SHARED_START EMPTY 0xfff0
    {
    }

    SHARED_RAM_END DATA_SHARED_END
    {
        *(SHARED_RAM_END)
    }
    
    ; mem_init writes a storeblock_struct at the end of kernel data,
    ; max size 32 bytes, so use 0x100 offset
   

   BOOT_STACK_ADDR (TCML_END - 0x100) OVERLAY
    {
        *(BOOT_STACK)
    }

    ; We don't use their stack or heap, but the tools expect this
    ; to be here, so we have a dummy placeholder.
    ARM_LIB_STACKHEAP (TCML_END - 0x100) OVERLAY EMPTY UNINIT 0x04
    {
    }
}

Regards,

Emmanuel

0 项奖励
回复