ISO 7816 support for MQX/Vybrid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISO 7816 support for MQX/Vybrid

Jump to solution
1,279 Views
MehmetAliIpin
Contributor V

Dear Sir/Madam,

It is explained that Vybrid serial port UART' support ISO 7816 EMV standart for smart card readers. I could not see it in MQX directories, does anybody know, if MQX supoort ISO 7816 EMV standart? or are there source codes for ISO 7816 for Vybrid/linux?

Best regards

Mehmet Ali Ipin

0 Kudos
Reply
1 Solution
721 Views
timesyssupport
Senior Contributor II

Hello Mehmet,

I reviewed MQX and Linux source - I saw header definitions for ISO 7816 in each, but not an actual implementation. You could check if the MQX team has any plan to implement ISO 7816 for Vybrid in MQX. Timesys could also help under a services agreement. Let me know if you have any questions.

Thanks,

Timesys Support

View solution in original post

0 Kudos
Reply
4 Replies
721 Views
terry_lv
NXP Employee
NXP Employee

Hi,

     Currently, what we mean to support ISO7816/EMV means that UART IP has meet the timing required for ISO7816/EMV.

     Latest UART IP should support full ISO7816/EMV timing and can pass EMV L1 test.

     MQX havn't supported ISO7816 driver yet and I don't know if there're any plan for this.

     But KSDK do have a plan to support ISO7816 and will have this in official release of next year.

     Thanks~~

Best regards

Terry

0 Kudos
Reply
722 Views
timesyssupport
Senior Contributor II

Hello Mehmet,

I reviewed MQX and Linux source - I saw header definitions for ISO 7816 in each, but not an actual implementation. You could check if the MQX team has any plan to implement ISO 7816 for Vybrid in MQX. Timesys could also help under a services agreement. Let me know if you have any questions.

Thanks,

Timesys Support

0 Kudos
Reply
721 Views
MehmetAliIpin
Contributor V

Thank you very much.

0 Kudos
Reply
721 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 Kudos
Reply