I2C3 hangs after several write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C3 hangs after several write

3,543 Views
carlovalgocela
Contributor III

Good Day!

I have added I2C3 in the kernel Linux-3.0.15-ts-armv71 with I2C3 clock set to 100Khz.

I'm having some issues with my A5 application were sending of I2C data results to SDA pin stuck to LOW.

This usually happens when a NACK is received. The only way to recover is to power reset the board.

I2C hangs SDA stay Low.pngI2C SDA stay Low.png

Is there a way to send a stop command when a NACK is received so that we can restart sending?

Labels (2)
Tags (1)
5 Replies

3,274 Views
timesyssupport
Senior Contributor II

Hello Carlo,

Are you able to, or have you already, provided your application in the Timesys Support queue for this issue? Are you able to do so, so our engineers can reproduce and investigate the behavior?

Thank you,

Timesys Support

0 Kudos
Reply

3,274 Views
timesyssupport
Senior Contributor II

Hello Carlo,

We are reviewing here, and will follow up if we are able to reproduce without your custom application.

Regards,

Timesys Support

3,274 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ do you have an update?

0 Kudos
Reply

3,274 Views
karina_valencia
NXP Apps Support
NXP Apps Support

reminder

Timesys Support do you have an update?

0 Kudos
Reply

3,275 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you attend this case?

0 Kudos
Reply