I want to connect FPGA and Vybrid with 32bit data bus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to connect FPGA and Vybrid with 32bit data bus

1,311 Views
ohmyjskim
Contributor I

Hello,

I want to connect FPGA and Vybrid with 32bit data bus and over 10bit address (acting like SRAM).

Vybrid series have 32-bit flexbus but must use multiplexing address and data.

If ddr3 slave interface can be implemented in FPGA and connect ddr3 interface of Vybrid, can it workable?

Labels (5)
0 Kudos
Reply
1 Reply

1,125 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  only special pins (DDR_xxx, controlled by DDRMC) should be used for DDR3.

Hardly FPGA based approach (via FlexBus) can provide reliable solution.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply