I want to calculate of ”Read freaquency calculations", "Max read frequency", "Hold timing"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I want to calculate of ”Read freaquency calculations", "Max read frequency", "Hold timing"

跳至解决方案
1,281 次查看
takashitakahash
Contributor III

Hi community.

I'm trying to calculate the VYBRIDRSERIESEC_Rev_7.PDF p60 "Read freaquency calculations","Max read frequency","Hold timing", but I don't know following values

Would you please teach me  measured in each of the same kind of value .

・Flash access time

・flash_access(min)

・flash_data_valid(min)

标签 (1)
0 项奖励
回复
1 解答
1,108 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As far I as I see the timings you need are dependant on the QSPI memory you are using.

Therefore you will need to check the timings in your memory.

For example

Frequency calculator guideline (Max read frequency): SCK > (Flash access time)max + (Tis)max

Tis allowed for our QSPI module is a min of 4.5ns.  But Flash access time may be found in the manufacturer datasheet.

/Alejandro

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,109 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As far I as I see the timings you need are dependant on the QSPI memory you are using.

Therefore you will need to check the timings in your memory.

For example

Frequency calculator guideline (Max read frequency): SCK > (Flash access time)max + (Tis)max

Tis allowed for our QSPI module is a min of 4.5ns.  But Flash access time may be found in the manufacturer datasheet.

/Alejandro

0 项奖励
回复