How to use nosigthresh of VYBRID RM of 61.6.27(VDEC_VSSGTH)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use nosigthresh of VYBRID RM of 61.6.27(VDEC_VSSGTH)

Jump to solution
1,110 Views
takashitakahash
Contributor III

Hi,community

Our customer want to detection of signal or nosignal of NTSC imput.

Signal detection use register of VDEC_VIDMOD field descriptions of  bit "0" Have signal to set "1".

And detection level use VDEC_VSSGTH field description of "nosigthresh".

Question

Would please tell me what mean nosigthresh step by step valu.

If set to 0x001,Is this detect noise voltage? or noise period?

There are set to 0x101 is wlong. noise detection.

But set to 0x111 is no ploblem noise is no detect.

Labels (1)
1 Solution
819 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
4 Replies
820 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
820 Views
richard_stulens
NXP Employee
NXP Employee

Hi Takahashi-san,

We are still working on the details, but we believe the 3-bit field defines the threshold level for the input signal.

If the setting is 'n', then the threshold level is 2 ^(n+1). ex. if nosigthresh is set to 0b010, the threshold is 2^3 = 8.

Best regards,

Richard

820 Views
karina_valencia
NXP Apps Support
NXP Apps Support

richard_stulens​ do you have an update?

0 Kudos
820 Views
richard_stulens
NXP Employee
NXP Employee

I think this is handled through the FAE's. This is the same project/issue as "VADC questions for NTSC input"

https://community.freescale.com/message/582045?et=watches.email.thread#582045

Regards,

Richard