How to set SSC function of PLL1 and PLL2 of SVF522XX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set SSC function of PLL1 and PLL2 of SVF522XX

ソリューションへジャンプ
1,408件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer want to use SSC function of PLL1 and PLL2 .Becouse There are noise issues.

I read  Vybrid RM of sect 9.4.2 Spred Spectrum but i could not be well understood. .

Do I get the recommended value to be set to specifically PLL1 and PLL2.

Frequency, width, step does not matter in the recommended settings.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,079件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

There is a document for iMX6 devices. enable the spread spectrum

The clocking of both devices are similar and I think it can help.

Are you trying to achieve an specific modulation frequency and depth?

Best Regards,

Alejandro

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,080件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

There is a document for iMX6 devices. enable the spread spectrum

The clocking of both devices are similar and I think it can help.

Are you trying to achieve an specific modulation frequency and depth?

Best Regards,

Alejandro

0 件の賞賛
返信