How to set GCC, MQX and eclipse for Vybrid VF3x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set GCC, MQX and eclipse for Vybrid VF3x

2,453 Views
POSterminalPCI_
Contributor II

Dear Sir/Madam,

Hello

I have gcc version 4.8.1 (which I think it has cross compile for ARM Cortex A5 ) into Ubuntu 12.4; eclipse juno for C/C++. I also have MQX 4.0.

I want to cross compile a simple hello world source for ARM Cortex A5 (for Vybrid VF3X). How can I establish a cross compile Project settings? Do you have any document/App Note which explains the steps or do you have a basic Project with make file for VF3X with MQX which I can built the Project with gcc ?


Best wishes.


Mehmet Ali Ipin.

Labels (3)
Tags (4)
2 Replies

1,879 Views
c0170
Senior Contributor III

Hello,

I would like to know what GCC toolchain and  what debugger are you using ?

Regards,

c1070

1,879 Views
POSterminalPCI_
Contributor II

Dear Martin,

Hello

Thank you for your interest,

I have GCC 4.8.1. I am not using any debugger yet. First I want to establish an environment to cross compile files for Vybrid (arm v7), with or without eclipse, then integrate the MQX. after MQX integrated, I will consider the debugger.

Best regards.

0 Kudos
Reply