How to implement soft reset on Vybrid running MQX?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to implement soft reset on Vybrid running MQX?

ソリューションへジャンプ
3,440件の閲覧回数
flaviocaduda
Contributor II

How do I implement a soft reset on Vybrid running MQX? On Cortex M I know that a specific register (AIRCR) is used for system wide reset from within software. Is there any similar way on the Cortex A5? Or is this done from the Cortex-M4 on the Vybrid? Anyone has an example they could share?

Regards,

Flavio

1 解決策
2,876件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi,

for software reset use SW_RST bit in SRC Control Register (SRC_SCR). See chapter 18.3.2 in Vybrid RM.

Regards

Rene

元の投稿で解決策を見る

5 返答(返信)
2,876件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Flavio,

In the below discussion you can get more information regarding software reset. Reset A5 without interfering on M4

Please keep us informed if using the SW_RST helped you.

/Alejandro

2,876件の閲覧回数
flaviocaduda
Contributor II

Thanks Rene, it worked. Yet there is an unwanted side effect. The MQX and IAR debugger don't keep synch after the reset. I suppose it is because there is no memory repair sequence after a soft reset, or IAR doesn't know what to do after the soft reset.

Regards,

Flavio Caduda

0 件の賞賛
返信
2,877件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi,

for software reset use SW_RST bit in SRC Control Register (SRC_SCR). See chapter 18.3.2 in Vybrid RM.

Regards

Rene

2,876件の閲覧回数
bfac
NXP Employee
NXP Employee

karinavalencia, can you help us expediting this request?

2,876件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

rendy can you help here?

0 件の賞賛
返信