How to enable Vybrid TCON Spread Spectrum?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable Vybrid TCON Spread Spectrum?

1,625 Views
mpfgregory
Contributor III

Our product fails EMI testing because of the display pixel clock. We're using a TFT with TTL interface, controlled by the DCU and TCON drivers. I wonder if it's possible to enable spread spectrum for the TCON module. From the VybridRM I don't understand how the pixel clock is generated. The TCON module has its own Timing Signal Generator (TSG). Is the TSG related to the Clock Controller Module (CCM)? If I enable spread spectrum for PLL1 or PLL2 in the CCM, will this affect the TSG? If not, is there another way to enable spread spectrum for the TCON module?

Thanks for your help

Michael

Labels (2)
0 Kudos
Reply
1 Reply

1,402 Views
mpfgregory
Contributor III

I've found the solution myself. You need to enable spread spectrum for the DCU, not the TCON. In CCM_CSCMR1 you can select PLL1_PFD2 as DCU clock. Then you can enable spread spectrum for PLL1 in ANADIG_PLL1_SS:

clrsetbits_le32(&anadig->pll1_ss, 0xffffffff, (1 << 15) | (4400 << 16) | 11);

0 Kudos
Reply