How to enable Ethernet on AutoEVB revC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable Ethernet on AutoEVB revC

1,268 Views
ioseph_martinez
NXP Employee
NXP Employee

Thanks to TsiChung we have now Ethernet working on our RevC AutoEVB boards, follow the next steps:

1.Add 1.5K ohm to R159 (top side, next Ethernet PHY)
2.SW12 pin 4 set to ON
3.No change for IOMUX pin configuration (settings that comes with u-boot)
4.Make sure to pull up on PHY reset pin (mw.l 40048088 001021be in u-boot)
5.Typed “mii info”, if it comes up quick and shows 100Base, then connection is good.

If you configure correctly your netmask, ipaddress you will be able to ping other devices as well.

Uboot version I am using:

U-Boot 2011.12-00548-gd2215dc-dirty (Mar 26 2013 - 16:59:44)

20130412_122523.jpg

Tags (3)
0 Kudos
Reply
1 Reply

1,050 Views
ioseph_martinez
NXP Employee
NXP Employee

Just to confirm, you must have a valid netmask and ipaddr if you want this to work on a network (at least the one I am using)

In my case I use:

setenv netmask 255.255.255.0

setenv ipaddr 10.112.102.100

saveenv

Then you can ping.

0 Kudos
Reply