Respected Colleagues,
how to make a script for automatic start of some Vybrid application after boot in the Timesys Linux, and where to implement call of that script ?
For example, after power failure, application have to start automatically.
Is it explained in some Timesys document?
Thanks in advance.
With best regards,
Dragan Kujovic
已解决! 转到解答。
Unless it has changed, look in /etc/init.d - you will find scripts named s* and k* - the s* scripts are executed in alphabetical order on startup (they must have x permission) and the k files are executed in alphabetical order on shutdown. Simply add your own script. Typically it runs last and make sure your command runs in background (ends with "&") if you want to continue to a shell prompt.
Unless it has changed, look in /etc/init.d - you will find scripts named s* and k* - the s* scripts are executed in alphabetical order on startup (they must have x permission) and the k files are executed in alphabetical order on shutdown. Simply add your own script. Typically it runs last and make sure your command runs in background (ends with "&") if you want to continue to a shell prompt.
Respected ed_nash
thanks to your suggestion I have managed to make and start my application trough script file at the and of boot.
To help others that have little knowledge as I have, I will elaborate this topic further.
In Timesys Factory folder (for example):
/timesys/pcl052/factory-20140113/build_armv7l-timesys-linux-gnueabi/rfs/etc/init.d
Make file with S*XX prefix where XX is the highest number in that folder. For example: S99_ACME
I have attached sample file, where you have to change path and file name you wish to start.
This file copy to /rfs/etc/init.d folder of your SD card.
With best regards,
Dragan Kujovic