How is the M4 booted with the Vybrid with M4 as primary?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How is the M4 booted with the Vybrid with M4 as primary?

跳至解决方案
1,638 次查看
jwu
Contributor I

How is the M4 booted with the Vybrid with M4 as primary? What's the difference between M4 as a primary and A5 as a primary in the hardware? Via fuse setting.

Thanks,

John

0 项奖励
回复
1 解答
1,179 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi John,

  The boot core is determined by which part number you buy. The device on the Vybrid tower board is an A5 primary device.

  What that means is that the A5 core runs all the BootROM code, and then jump to your user code. You have to explicitly enable the M4 core in your user code to begin using it.

  Likewise on an M4 primary part, the M4 core would run all the BootROM code and then jump to user code. The A5 core would have to be explicitly enabled in your user code to begin using it.

  See this thread for more information on emulating an M4 primary chip on the tower system: M4 Primary Emulation

-Anthony

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,180 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi John,

  The boot core is determined by which part number you buy. The device on the Vybrid tower board is an A5 primary device.

  What that means is that the A5 core runs all the BootROM code, and then jump to your user code. You have to explicitly enable the M4 core in your user code to begin using it.

  Likewise on an M4 primary part, the M4 core would run all the BootROM code and then jump to user code. The A5 core would have to be explicitly enabled in your user code to begin using it.

  See this thread for more information on emulating an M4 primary chip on the tower system: M4 Primary Emulation

-Anthony

0 项奖励
回复