Hello,
we need some hints to get our TWR_VF65GS10 to boot via qspi and SRAM (not XIP image).
Freescale tells us how to setup the IVT and Boot Data (see Figure 19-20 of the Vybrid Reference Manual Rev 7, 06/2014).
However, we cannot find out how to tell the boot rom program where our image is located in the qspi so it can copy it into internal ram.
IVT entry points to the address of the first instruction of the image at the destination memory (internal RAM)
Boot Data start points to the start address of the image in the destination memory (internal RAM)
Boot Data length length of the image
Location of
Image in qspi to be
copied to Boot Data
start ????
Which part am I missing? Is there a better documentation as the one mentioned above? Are there actually examples where I can
get the required Information?
Ralf
已解决! 转到解答。