High-level input higher than ovdd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

High-level input higher than ovdd

跳至解决方案
4,020 次查看
shouminliu
Contributor II

Dear Sir or Madam:

we are evaluating multiple options to power the Vybrid using a single 3.3V supply. We are looking into a 1.5V-controlled LDO as the sequencing device shown in the block diagram attached. However, we have some concerns about the Vybrid. Could you please comment on our questions below?

  1. We realize that there will be a little dropout voltage between 3.3V_P and 3.3V_S anyway. In our application, 3.3V_S will power the  Vybrid and 3.3V_P will power some peripheral digital electronics around it. It is possible that a logic-high input (powered by 3.3V_P) is higher than 3.3V_S that powers the Vybrid GPIO. The data sheet says that the high-level input has a max. value of ovdd, which is 3.3V_S in our case. Will a “higher-than-3.3V_S” cause any damage or malfunctions? What do you think?
  2. In the configuration shown in the block diagram, peripheral electronics will be powered on before the Vybrid (3.3V_P turns on before 3.3V_S). In case there are high-level inputs at some GPIO pins before 3.3V_S is on, we guess these inputs will be shunted to the internal 3.3V rail by the internal protection Schottky diodes. If this is true, the Vybrid 3.3V rail is virtually powered by the high-level input minus the voltage drop on the Schottky diodes. Will this phenomenon cause the Vybrid to enter a “partially-powered” state and malfunction?

Please kindly let us know what you think.

Thanks and regards,

Shoumin

标签 (3)
0 项奖励
回复
1 解答
3,778 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,779 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
3,784 次查看
art
NXP Employee
NXP Employee

Q. Will a “higher-than-3.3V_S” cause any damage or malfunctions?

A. Yes, it can cause an excessive input current and even I/O buffer damage.

Q. Will this phenomenon cause the Vybrid to enter a “partially-powered” state and malfunction?

A. Yes, this can cause a malfunction. The general requirement is that no I/O pins must be externally driven until the processor is powered on.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复