GPC in about "Vybrid Reference Manual, Rev. 7, 06/2014"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GPC in about "Vybrid Reference Manual, Rev. 7, 06/2014"

跳至解决方案
1,651 次查看
soichiyamamoto
Contributor V

Hi,

That's a question from a customer.

I will ask a question about "Vybrid Reference Manual, Rev. 7, 06/2014".

The following register is deleted by a manual.

・GPC_IMR2

・GPC_IMR3

・GPC_ISR2

・GPC_ISR3

Does it mean that I cannot use these registers?

Will it be explained in Errata?

Best Regards,

soichi


标签 (1)
0 项奖励
回复
1 解答
1,216 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Soichi,

There is missing also GPC_PGCR and GPC_PGSR. Unfortunately description of those register is not present due to the mistake in final RM generation at documentation department. Should be corrected soon.

For you convenience - attached is the GPC chapter from RM v.5

/Jiri

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,217 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Soichi,

There is missing also GPC_PGCR and GPC_PGSR. Unfortunately description of those register is not present due to the mistake in final RM generation at documentation department. Should be corrected soon.

For you convenience - attached is the GPC chapter from RM v.5

/Jiri

0 项奖励
回复
1,216 次查看
soichiyamamoto
Contributor V

Dear Jiri,

Thank you for reply.

I close the thred.

Bset Regards,

soichi

0 项奖励
回复