GPC in about "Vybrid Reference Manual, Rev. 7, 06/2014"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPC in about "Vybrid Reference Manual, Rev. 7, 06/2014"

ソリューションへジャンプ
1,764件の閲覧回数
soichiyamamoto
Contributor V

Hi,

That's a question from a customer.

I will ask a question about "Vybrid Reference Manual, Rev. 7, 06/2014".

The following register is deleted by a manual.

・GPC_IMR2

・GPC_IMR3

・GPC_ISR2

・GPC_ISR3

Does it mean that I cannot use these registers?

Will it be explained in Errata?

Best Regards,

soichi


ラベル(1)
0 件の賞賛
返信
1 解決策
1,329件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hi Soichi,

There is missing also GPC_PGCR and GPC_PGSR. Unfortunately description of those register is not present due to the mistake in final RM generation at documentation department. Should be corrected soon.

For you convenience - attached is the GPC chapter from RM v.5

/Jiri

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,330件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hi Soichi,

There is missing also GPC_PGCR and GPC_PGSR. Unfortunately description of those register is not present due to the mistake in final RM generation at documentation department. Should be corrected soon.

For you convenience - attached is the GPC chapter from RM v.5

/Jiri

0 件の賞賛
返信
1,329件の閲覧回数
soichiyamamoto
Contributor V

Dear Jiri,

Thank you for reply.

I close the thred.

Bset Regards,

soichi

0 件の賞賛
返信