GPC in about "Vybrid Reference Manual, Rev. 7, 06/2014"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPC in about "Vybrid Reference Manual, Rev. 7, 06/2014"

Jump to solution
1,631 Views
soichiyamamoto
Contributor V

Hi,

That's a question from a customer.

I will ask a question about "Vybrid Reference Manual, Rev. 7, 06/2014".

The following register is deleted by a manual.

・GPC_IMR2

・GPC_IMR3

・GPC_ISR2

・GPC_ISR3

Does it mean that I cannot use these registers?

Will it be explained in Errata?

Best Regards,

soichi


Labels (1)
0 Kudos
Reply
1 Solution
1,196 Views
jiri-b36968
NXP Employee
NXP Employee

Hi Soichi,

There is missing also GPC_PGCR and GPC_PGSR. Unfortunately description of those register is not present due to the mistake in final RM generation at documentation department. Should be corrected soon.

For you convenience - attached is the GPC chapter from RM v.5

/Jiri

View solution in original post

0 Kudos
Reply
2 Replies
1,197 Views
jiri-b36968
NXP Employee
NXP Employee

Hi Soichi,

There is missing also GPC_PGCR and GPC_PGSR. Unfortunately description of those register is not present due to the mistake in final RM generation at documentation department. Should be corrected soon.

For you convenience - attached is the GPC chapter from RM v.5

/Jiri

0 Kudos
Reply
1,196 Views
soichiyamamoto
Contributor V

Dear Jiri,

Thank you for reply.

I close the thred.

Bset Regards,

soichi

0 Kudos
Reply