Thank you for the information. I don't have a specific problem with Vybrid. I am looking for a processor that can do data transfers using UARTS, USB flash drive, and 10/100 Ethernet. All transfers are simultaneous. I'd like to have two UARTS running full duplex at 1Mbps and would like to write data to a USB flash drive at about 4 MB/sec, and send and receive data TCP/IP at about 2 MB/sec. I have been looking at Cortex M4/M7 MCU's, but I'm not sure they can keep up with these data rates. I've also been looking at the A9 processors. I think A9 can do the data rates, but they have more features than I really need. I think A9 is also more power hungry than I want. The Vybrid looks like it may be a good middle ground, but I think the A5 was intended to run Linux, and maybe the Vybrid A5 running Linux can meet my performance requirements, but if it can't I was thinking MQX running on the A5 might be a good fall back solution.
 
					
				
		
 karina_valencia
		
			karina_valencia
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		SergioSolis are you able to continue with the follow up?
 
					
				
		
 SergioSolis
		
			SergioSolis
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Well, I haven't run MQX in the Vybrid A5.. alejandrolozano you have more experience with MQX, have you used the A5 with MQX?
 
					
				
		
 alejandrolozan1
		
			alejandrolozan1
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
Yes, theres support in MQX for the CA5. There very basic examples found in the< MQX_INSTALLATION_FOLDER>/mqx/examples/ That you can use as reference. There are multiple exmaples working in IAR, DS-5 or even using Makefiles with the command line.
Are you having some kind of problem?
Best Regards,
Alejandro
 
					
				
		
 SergioSolis
		
			SergioSolis
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		It does support the A5 core, please take a look at the following document for a detailed version list and their support.
http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/MQXFS.pdf