Hi
I am working on Vybrid TWRVF65GS10 board and my code reside in internal RAM. I had initialized the SDRAM (0x80000000) successfully. Now I want to disable DDR but could not. Here is my sequence.
1. Disable Clock Gating WRITE32(0x4006B058, READ32(0x4006B058) & 0xCFFFFFFF); // Disable DDR Clock Gating 6_14
2. Reset IOMUX settings to their reset values. i.e. Reset Value is 0x10060 and Write this value in all IOMUX registers ranges [21C-2E0]
After this, if I write a value 0xdeadbeef to a address 0x8000000, It is read back (Value should be not be written because DDR should be closed after these two steps.).
What is missing in my settings?
Regards
Solved! Go to Solution.
Hi,
Would you be nice enough to provide more details about your application? Is there any reason to disable the DDR on the fly?
Regards,
Alejandro
muhammad_qasim do you have the information requested?