DS5 Vybrid VF6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DS5 Vybrid VF6

Jump to solution
1,374 Views
peralesserrano
Contributor I

hello,

I want to start working with processors vybrid but I see you have less documentation than processors i.mx

would want to know if it is possible to program and debug applications VF6 with DS5 community edition, is it possible to work with the core M4 and A5?

Labels (5)
0 Kudos
1 Solution
1,019 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
3 Replies
1,020 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
1,022 Views
b47504
NXP Employee
NXP Employee

Ds5 can be used to debug M4 and A5.

0 Kudos
1,021 Views
jiri-b36968
NXP Employee
NXP Employee

Hi Serrano,

regarding debug:

please look at this dual debug connection

you can see a video for it https://www.youtube.com/watch?feature=player_embedded&v=djExDHsBa5w (in newest DS-5 the connection configuration is little bit different)

when you by TWR-VF65 tower module then you will get license for DS-5 with limited code size (256k or 1M). Or you can by a kit: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-VF65GS10&fsrch=1

/Jiri