I encountered an issue with DMA running in SPI0.
Currently in MQX, I'm running an application that gathers data via SPI0 DMA.
Data gathering should not be interrupted. Its function is gather data all the time.
During the data gathering i got an error see below:
IO_IOCTL_SPI_READ_WRITE ... drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (49)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (48)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (48)
I already disabled the DMA for SPI0 in Linux by disabling CONFIG_SPI_MVF_DSPI_EDMA.
Still the issue occurred.
I added some code to display the address, irq,dev_id and intr when the issue occurs.
Here is the result:
----------------------------------------------------------------------------------------------------------------------
drivers/dma/mvf_edma.c:mcf_
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: Invalid channel 31. addr=0xf20b8000, irq=42, dev_id=8a000000, intr=0x00000000
-------------------------------------------------------------------------------------------------------------------------
also i tried to display the interrupts trying to get who are using the irq 42
CPU0
36: 0 GIC mvf_sema4_handler
40: 0 GIC mcf_edma
41: 0 GIC mcf_edma
42: 0 GIC mcf_edma
43: 0 GIC mcf_edma
解決済! 解決策の投稿を見る。
Hello rendy and karinavalencia
any updates?
For now we edited the sample SPI MQX code and added some code to have an infinite loop. See attached file.
rw.BUFFER_LENGTH = 10;
rw.WRITE_BUFFER = (char *)send_buffer;
rw.READ_BUFFER = (char *)recv_buffer;
printf ("IO_IOCTL_SPI_READ_WRITE ... ");
while(1)
{
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_READ_WRITE, &rw))
{
printf ("OK\n");
}
else
{
printf ("ERROR\n");
}
}
When running the MQX file the error occured.
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (49)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (48)
Any idea what might cause the issue?
Today we tried a test where only MQX is running by loading via DS5.
In the 2 hours testing the issue didn't occur.
timesyssupport and rendy any idea ??
timesyssupport, rendy,
Have you had a chance to take a look at this problem. Any ideas are welcome.
Best Regards,
Alejandro
Hello All,
I tried to check if the issue will still occur on the latest kernel 3.13
And the issue occurred immediately with a Kernel Panic see attached picture.
# cat /proc/interrupts
CPU0
27: 1810 GIC 27 gt
36: 0 GIC 36 mvf_sema4_handler
40: 0 GIC 40 eDMA tx
41: 0 GIC 41 eDMA err
42: 0 GIC 42 eDMA tx
43: 0 GIC 43 eDMA err
I have reproduced the error. It has been difficult to debug the problem because of Linux. I wonder if you have seen this before.
/Alejandro
timesyssupport can you comment please?
Hello Karina,
I have asked our Vybrid maintainer to review, and follow up. He is currently working through 3.13 kernel porting, as well as DMA and MQX issues. Unfortunately I am not able to immediately provide support. Thanks for your patience.
Timesys Support
Hello timesyssupport karinavalencia alejandrolozano
I edited the mvf_edma.c in Linux to reroute the DMA1 to DMA0 and observed the following:
1. The data gathering via DMA works fine but the error prompt still occurs.
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (31)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (49)
drivers/dma/mvf_edma.c:mcf_edma_isr: No handler for DMA channel (48)
2. I then tried to remove the error message either of the following:
- filter DMA channel 31, 49 and 48 or
- commenting out ERR(" No handler for DMA channel (%d)\n", channel); in the mcf_edma_isr()
Result: the data gathering failed or stop gathering
What i think is when the printing the error message, the error in the isr was not being catered or ignored.
And when the Linux is running fast by removing the print out it is being processed. There might be an issue in processing
the ISR.
Hello carlovalgocela and karinavalencia,
I believe we have determined in the same ticket in the Timesys queue, this is using MQX 4.1.1 which is not currently compatible with either Linux 3.0.15, or 3.13 and associated MCC for Vybrid. If this is reproduce-able using MQX 4.0.2, we can investigate.
Thank you,
Timesys Support
Hi timesyssupport,
Does that mean that only MQX 4.0.2 is compatible with Linux?
carlovalgocela, which MQX version are you using?
Best Regards,
Alejandro
Hello alejandrolozano
I'm using MQX 4.1.1 as DMA is supported in DSPI0.
MCC is working fine with Linux version 3.0.15-ts-armv7l and the MQX 4.1.1
As we've previously noted, MQX 4.1.1 is not supported against the 3.0.15 kernel; while it can be made to work, it's not recommended.
We are only able to support issues with MQX 4.0.2 at this time, as we are concentrating efforts on the 3.13 kernel, and corresponding MQX/MCC support.
Thank you,
Timesys Support
timesyssupport do you have specific timeline when the newer MQX will be supported?
Based on my test, i found out when the function mcf_edma_isr() doesn't respond a valid result (IRQ_HANDLED)
It will stop the data gathering and make the Linux wait for a valid handler for ISR.
For now, the temporary solution i used to make it work is filter out when DMA Channel = 31, 48 and 49 and return IRQ_HANDLED.
This is not a good and clean solution.
timesyssupport - CAn you guide me what the DMA channel 31,48,49 corresponds to what devices?
Thanks
timesyssupport do you have an update?
Hello Karina,
We have been working with Carlo via our internal support. We will keep the community updated on the progress on this issue. We currently have Carlo's MQX binary, but are unable to reproduce the issue.
Thanks,
Timesys Support
Thanks for sharing the progress.
Timesys Support can you share the status?
Hello Karina,
We are still working to reproduce this issue on our end. If we are able to identify the issue and resolve it, we will follow up.
Regards,
Timesys Support
Timesys Support can you share the status?