Cryptographic Acceleration and Assurance Module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Cryptographic Acceleration and Assurance Module

跳至解决方案
4,252 次查看
ngsari
Contributor II

I like to use CAAM Register interface (IP bus). But there is almost no information in the SECURITY documentation.
(The document is full of how to use those modules but lack of details.)
How can I access those registers with C ? (Or Assembly if I realy have to)
CAAM Status Register
RNG TRNG Status Register
RNG DRNG Status Register

标签 (5)
1 解答
3,168 次查看
matthieugaboria
Contributor II

Hello NG Sari,

Some information about these registers are page 628/629 of the VYBRIDSRM (RNG TRNG Status Register, RNG DRNG Status Register).

The CAAM base address can be found section 2.9 of the same document.

I hope it helps.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,168 次查看
billpringlemeir
Contributor V

There are also Linux kernel drivers which might also be helpful; it has some sample source.  The same CAAM engine is used on some iMx devices.

3,168 次查看
jackblather
Senior Contributor I

Bill,

I looked at that link and example source isn't there.

On further research, I understand that the CAAM is accessed via the Linux Crypto drivers. Do you know where I can find examples on how to use this?

Thanks.

0 项奖励
回复
3,168 次查看
billpringlemeir
Contributor V

The link is to a Linux Driver that uses the CAAM.  I don't know what you mean by example.  The CAAM is extremely complex.  The Linux CAAM driver shows how to use the registers (DECOs, Job rings and blobs) to do something.  I referenced it as a working example of how to use the registers; together with the documentation it can be helpful.  The user-space interface will depend on your Linux version.  wikipedia.org, lwn article, and the current Linux crypto api might be useful.  OpenSSL and others may possibly have a configuration to use this.  At least it is possible to implement an OpenSSL crypto interface what would use the CAAM to accelerate things.

0 项奖励
回复
3,168 次查看
ngsari
Contributor II

Thank you Bill. It's very helpfull. That saves me from a lot pain and time :smileyhappy:

0 项奖励
回复
3,169 次查看
matthieugaboria
Contributor II

Hello NG Sari,

Some information about these registers are page 628/629 of the VYBRIDSRM (RNG TRNG Status Register, RNG DRNG Status Register).

The CAAM base address can be found section 2.9 of the same document.

I hope it helps.

0 项奖励
回复
3,168 次查看
ngsari
Contributor II

Thank you so much :smileyhappy:

0 项奖励
回复