Can we use the VADC as fast ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use the VADC as fast ADC

Jump to solution
1,807 Views
davidwightman
Contributor II

I am curious if it is possible to use the VADC as a fast acting ADC, instead of for video.  Basically to get access to the VADC_DATAn before it gets to the Video Decoder.  We need an ADC that is in the same range as the 66.5Mbps rather than the 1Mbps general purpose ADC.

pastedImage_1.png

Labels (1)
0 Kudos
Reply
1 Solution
1,560 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,561 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,561 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Davin,

this would be great feature, but unfortunately it is not possible.

pastedImage_0.png

As you can see on the picture, a result from conversion goes directly to Video decoder. Only decoded data are available at the output of Video decoder. If used as fast ADC data cannot be decoded - so we do not get any output.

/Jiri