Can Vybrid boot from the only QSPI_B?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can Vybrid boot from the only QSPI_B?

Jump to solution
1,842 Views
Hiroki
NXP Employee
NXP Employee

Hi,

Can Vybrid boot from a QSPI Flash connected only the QSPI_B?

When the QSPI boot, First, the Vybrid set the pin mux and tries to get the QSPI configuration parameter from all Flash.

QSPI_A is always enabled but the optional configuration is that QSPI_B is enabled. So I think the Vybrid cannot boot from the only QSPI_B flash. Is it correct?

Labels (3)
0 Kudos
Reply
1 Solution
1,401 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Hiroki,

  That's correct, you must always boot from QSPI_A. You can use QuadSPI0 or QuadSPI1, as that is selected by fuses, but on QuadSPI0 you have to have all the information in QuadSPI0_A.

  See this thread for more information on QuadSPI booting. Parallel QuadSPI

-Anthony

View solution in original post

0 Kudos
Reply
1 Reply
1,402 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Hiroki,

  That's correct, you must always boot from QSPI_A. You can use QuadSPI0 or QuadSPI1, as that is selected by fuses, but on QuadSPI0 you have to have all the information in QuadSPI0_A.

  See this thread for more information on QuadSPI booting. Parallel QuadSPI

-Anthony

0 Kudos
Reply