Can Vybrid boot from the only QSPI_B?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can Vybrid boot from the only QSPI_B?

跳至解决方案
1,837 次查看
Hiroki
NXP Employee
NXP Employee

Hi,

Can Vybrid boot from a QSPI Flash connected only the QSPI_B?

When the QSPI boot, First, the Vybrid set the pin mux and tries to get the QSPI configuration parameter from all Flash.

QSPI_A is always enabled but the optional configuration is that QSPI_B is enabled. So I think the Vybrid cannot boot from the only QSPI_B flash. Is it correct?

标签 (3)
0 项奖励
回复
1 解答
1,396 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Hiroki,

  That's correct, you must always boot from QSPI_A. You can use QuadSPI0 or QuadSPI1, as that is selected by fuses, but on QuadSPI0 you have to have all the information in QuadSPI0_A.

  See this thread for more information on QuadSPI booting. Parallel QuadSPI

-Anthony

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,397 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Hiroki,

  That's correct, you must always boot from QSPI_A. You can use QuadSPI0 or QuadSPI1, as that is selected by fuses, but on QuadSPI0 you have to have all the information in QuadSPI0_A.

  See this thread for more information on QuadSPI booting. Parallel QuadSPI

-Anthony

0 项奖励
回复