Can I use the regular JTAG interface to debug both the A5 and M4 cores on the Vf6XX pocessor or do I need the trace port?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use the regular JTAG interface to debug both the A5 and M4 cores on the Vf6XX pocessor or do I need the trace port?

1,012件の閲覧回数
jamesherrera
Contributor II

I need some of the pins associated with the trace port for my design and need to know if I can debug with just the Vybrid standard interface using the 20 pin header.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

582件の閲覧回数
naoumgitnik
Senior Contributor V

Just rephrasing Jiri, "Yes, you can".

/Naoum.

0 件の賞賛
返信

582件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hi James,

for debug both cores the trace port /lines are not needed.

/Jiri

0 件の賞賛
返信