Can I use the regular JTAG interface to debug both the A5 and M4 cores on the Vf6XX pocessor or do I need the trace port?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use the regular JTAG interface to debug both the A5 and M4 cores on the Vf6XX pocessor or do I need the trace port?

1,410 Views
jamesherrera
Contributor II

I need some of the pins associated with the trace port for my design and need to know if I can debug with just the Vybrid standard interface using the 20 pin header.

Labels (4)
0 Kudos
Reply
2 Replies

980 Views
naoumgitnik
Senior Contributor V

Just rephrasing Jiri, "Yes, you can".

/Naoum.

0 Kudos
Reply

980 Views
jiri-b36968
NXP Employee
NXP Employee

Hi James,

for debug both cores the trace port /lines are not needed.

/Jiri

0 Kudos
Reply