Cache, set associate to direct mapped

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Cache, set associate to direct mapped

跳至解决方案
5,284 次查看
hjk
Contributor III

I read this on the ARM programmer guide

"You can lock the replacement algorithm on a way basis, enabling the associativity to be reduced from eight-way down to one-way, direct mapped."

Register 9 is the lockdown register, but I don't know how to use it, I saw "MRC p15,0,<Rd>,c9,c0,0" on ARM website, I have no idea how exactly it was used.

can someone provide an example of what exactly should I put in Rd, and how do I determine it is a read or write?

Thanks,

标签 (4)
0 项奖励
回复
1 解答
4,919 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,920 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
4,920 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Timesys Support do you have an update?

0 项奖励
回复
4,920 次查看
timesyssupport
Senior Contributor II

Hi,

The commands 'MRC' and 'MCR' are used to specify if its a read or a write operation. MRC stands for "send a command to a coprocessor and get some data back" and MCR is "send a command to a coprocessor and pass some data along".

Rd is the core register and its contents must be the value needed to be set in the register. I will update you with the example commands soon, meanwhile please refer the below link for more information  "ARM Information Center ".

Thanks,

Timesys Support.

4,920 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help here?

0 项奖励
回复