CMIS-DSP on Vybrid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMIS-DSP on Vybrid

Jump to solution
1,829 Views
carlovalgocela
Contributor III

Hello

I have read CMSIS-DSP library in Freescale (http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4489.pdf).

I would like to know if this is supported in Vybrid VF6xxx

As what i read on the document, examples are for Kinetis.

What libraries do i need to add.

Current setup:

- DS5 v5.19

- OS (Ubuntu 14 and Windows 7)

- Freescale MQX 4.0.2

Labels (3)
0 Kudos
Reply
1 Solution
1,596 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,597 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,599 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Carlo,

As you can see in the app note in IAR only a check box and a header found in the IAR folder installation are needed. But you can download the package from arm http://www.arm.com/products/processors/cortex-m/cortex-microcontroller-software-interface-standard.p...

Please notice that the libraries are only for Cortex M4.

0 Kudos
Reply