CMIS-DSP on Vybrid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,779件の閲覧回数
carlovalgocela
Contributor III

Hello

I have read CMSIS-DSP library in Freescale (http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4489.pdf).

I would like to know if this is supported in Vybrid VF6xxx

As what i read on the document, examples are for Kinetis.

What libraries do i need to add.

Current setup:

- DS5 v5.19

- OS (Ubuntu 14 and Windows 7)

- Freescale MQX 4.0.2

ラベル(3)
0 件の賞賛
返信
1 解決策
1,546件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,547件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
1,549件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Carlo,

As you can see in the app note in IAR only a check box and a header found in the IAR folder installation are needed. But you can download the package from arm http://www.arm.com/products/processors/cortex-m/cortex-microcontroller-software-interface-standard.p...

Please notice that the libraries are only for Cortex M4.

0 件の賞賛
返信