Board Revision of TWR-VF65GS10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board Revision of TWR-VF65GS10

Jump to solution
1,381 Views
pengcheng
Contributor III

I am using the TWR-VF65GS10 board currently and will write a hardware description to customer. But i don't know how to read the revision of the board, which label on pcb should i read as board revision? Thanks!

Add information:

There are three labels on the back of the board.

SCH-27442 REVH  -  I think this should be schematic revision

RV14210237   

700-27442 REV J1

Labels (1)
0 Kudos
Reply
1 Solution
1,210 Views
Yuri
NXP Employee
NXP Employee

Hello,

SCH-27442 REVH - schematic revision.

700-27442 REV J1 - board revision.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

----------------------

View solution in original post

2 Replies
1,211 Views
Yuri
NXP Employee
NXP Employee

Hello,

SCH-27442 REVH - schematic revision.

700-27442 REV J1 - board revision.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

----------------------

1,210 Views
pengcheng
Contributor III

Thank you very much

0 Kudos
Reply