Alternate for external NPN ballast transistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Alternate for external NPN ballast transistor

ソリューションへジャンプ
1,715件の閲覧回数
mnw
Contributor II

The tower board uses a NJD2873T4 for this, but we are looking for a smaller part in our design.  Is there a specification for what is required for this, or any other recommendations?

Thanks.

0 件の賞賛
返信
1 解決策
1,442件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Martin,

  We're working on creating a specification to put into the datasheet, as well as looking into alternative methods to reduce the current consumption on the ballast transistor. Unfortunately we don't have those at the moment yet, but will update everyone once it's ready

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,443件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Martin,

  We're working on creating a specification to put into the datasheet, as well as looking into alternative methods to reduce the current consumption on the ballast transistor. Unfortunately we don't have those at the moment yet, but will update everyone once it's ready

0 件の賞賛
返信
1,442件の閲覧回数
mnw
Contributor II

Hi

I see there has been an update in the docs on this issue.  0.85A seems quite high for the max current and still requires quite a big part. Do you have any more information on where this current number comes from?

Thanks.

0 件の賞賛
返信