Access serial port on TWR-Ser2 from Timesys?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Access serial port on TWR-Ser2 from Timesys?

Jump to solution
1,981 Views
tomaszsliwinski
Contributor III

Hello,

Can I access serial port on TWR-Ser2 from Timesys?  It is ttyc: on MQX but I need to access if from Timesys

This is from straight C.  I have the code but need to know the name of the port on the TimeSys side.

thanks

Thomas

Tags (2)
0 Kudos
Reply
1 Solution
1,804 Views
timesyssupport
Senior Contributor II

Hello Thomas,

The serial console in Linux enumerates as ttymxc1; in the 3.13 kernel the driver is located at /drivers/tty/serial/imx.c

Regards,

Timesys Support

View solution in original post

4 Replies
1,805 Views
timesyssupport
Senior Contributor II

Hello Thomas,

The serial console in Linux enumerates as ttymxc1; in the 3.13 kernel the driver is located at /drivers/tty/serial/imx.c

Regards,

Timesys Support

1,804 Views
tomaszsliwinski
Contributor III

great! thanks

0 Kudos
Reply
1,804 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you attend this case?

0 Kudos
Reply
1,804 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Timesys Support do you have an update?

0 Kudos
Reply