Access serial port on TWR-Ser2 from Timesys?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Access serial port on TWR-Ser2 from Timesys?

跳至解决方案
1,838 次查看
tomaszsliwinski
Contributor III

Hello,

Can I access serial port on TWR-Ser2 from Timesys?  It is ttyc: on MQX but I need to access if from Timesys

This is from straight C.  I have the code but need to know the name of the port on the TimeSys side.

thanks

Thomas

标记 (2)
0 项奖励
回复
1 解答
1,661 次查看
timesyssupport
Senior Contributor II

Hello Thomas,

The serial console in Linux enumerates as ttymxc1; in the 3.13 kernel the driver is located at /drivers/tty/serial/imx.c

Regards,

Timesys Support

在原帖中查看解决方案

4 回复数
1,662 次查看
timesyssupport
Senior Contributor II

Hello Thomas,

The serial console in Linux enumerates as ttymxc1; in the 3.13 kernel the driver is located at /drivers/tty/serial/imx.c

Regards,

Timesys Support

1,661 次查看
tomaszsliwinski
Contributor III

great! thanks

0 项奖励
回复
1,661 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you attend this case?

0 项奖励
回复
1,661 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Timesys Support do you have an update?

0 项奖励
回复