Access serial port on TWR-Ser2 from Timesys?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Access serial port on TWR-Ser2 from Timesys?

ソリューションへジャンプ
1,991件の閲覧回数
tomaszsliwinski
Contributor III

Hello,

Can I access serial port on TWR-Ser2 from Timesys?  It is ttyc: on MQX but I need to access if from Timesys

This is from straight C.  I have the code but need to know the name of the port on the TimeSys side.

thanks

Thomas

タグ(2)
0 件の賞賛
返信
1 解決策
1,814件の閲覧回数
timesyssupport
Senior Contributor II

Hello Thomas,

The serial console in Linux enumerates as ttymxc1; in the 3.13 kernel the driver is located at /drivers/tty/serial/imx.c

Regards,

Timesys Support

元の投稿で解決策を見る

4 返答(返信)
1,815件の閲覧回数
timesyssupport
Senior Contributor II

Hello Thomas,

The serial console in Linux enumerates as ttymxc1; in the 3.13 kernel the driver is located at /drivers/tty/serial/imx.c

Regards,

Timesys Support

1,814件の閲覧回数
tomaszsliwinski
Contributor III

great! thanks

0 件の賞賛
返信
1,814件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you attend this case?

0 件の賞賛
返信
1,814件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Timesys Support do you have an update?

0 件の賞賛
返信