About the Note of 8.1 Power sequencing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the Note of 8.1 Power sequencing

1,283件の閲覧回数
keisukewatanabe
Contributor III

According to datasheet, There is listed that is "At power down, it should be checked that 1.2V falls before 3.3V.".

Does Vybrid have this function? Should my customer do it?

Document Number: VYBRIDRSERIESEC Rev.5

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,126件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Keisuke,

Yes, Vybrid itself takes care of its 1.2V power rail, the only requirement being to NOT connect an external 1.2V source to it (i.e. following our datasheet and reference design).

Regards, Naoum Gitnik.

0 件の賞賛
返信

1,126件の閲覧回数
keisukewatanabe
Contributor III

I'm sorry, explanation is poor.

I want to know whether there is the way to drop 1.2V intentionally.

Best regards,

Keisuke Watanabe

0 件の賞賛
返信

1,126件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Keisuke,

Just an example of how the designer can violate this rule - if the capacitance on the 1.2V rail is too high (way higher than recommended in our documentation), then when powering down, the actual rail voltage might be decreasing so slowly that at some point would appear to be higher than that of the 3.3V rail one decreasing faster.

Regards, Naoum Gitnik.