Where is the tool VIT Text-to-Model?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the tool VIT Text-to-Model?

5,417 Views
yugandhar421
Contributor II

Hi,

I want to try the Text to Model tool which is used to generate VIT AI model for custom wake word and custom voice commands. In the video demo available at MCU Tech Minutes: Text-to-Model Demo Using NXP’s Voice Intelligent Library (VIT) on i.MX RT1170 MCUs they are talking about the Text to Model tool, but no link provided from where it can be downloadable.

 

More than 4 hours I searched in Google and NXP website, but no where I can find this tool, all docs only I can see with terms VIT and Text to Model. It is better if NXP people provides the links of software/tools mentioned in the demo, which saves programmers time atleast.

 

If anybody knows about this tool please help me.

 

Thanks,

Yugandhar

0 Kudos
Reply
3 Replies

5,119 Views
Laurent_P
NXP Employee
NXP Employee

Hello Yugandhar,

 

The VIT model generation tool is now available online at   https://vit.nxp.com/#/

 

 

Thanks,

Laurent 

 

0 Kudos
Reply

5,353 Views
nxf49874
NXP Employee
NXP Employee

@FelipeGarcia  Is the VIT SDK open? If yes, where can I download it? I checked the SDK V2.10.0 for RT1170, but VIT project is not found.

0 Kudos
Reply

5,403 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Yugandhar,

The tool is not public that is why is not located in our website. Sorry for the inconvenience.

Best regards,

Felipe

0 Kudos
Reply