Question 1: Will the RT1050 will be supported by either the SLN-LOCAL-RD or the Voice Intelligence Technology (VIT) platform?
Question 2: Looking to confirm the SLN-LOCAL2-RD supports the the Industrial speed grade (528MHz) of the RT106S - or is the consumer speed grade required?
解決済! 解決策の投稿を見る。
First, please note either SLN-LOCAL-RD or SLN-LOCAL2-RD needs the special part to support rather than the general part from business perspective.
So for SLN-LOCAL-RD, the RT105S is the right part for selection. About VIT, only RT1060 is supported on RT10xx families from current on-chip SRAM requirements.
About SLN-LOCAL2-RD, RT106S has both commercial grade part and industrial grade part. Thanks!
@MikeBrennan do you require more information/help here?
Thanks @MikeBrennan for letting us know.
First, please note either SLN-LOCAL-RD or SLN-LOCAL2-RD needs the special part to support rather than the general part from business perspective.
So for SLN-LOCAL-RD, the RT105S is the right part for selection. About VIT, only RT1060 is supported on RT10xx families from current on-chip SRAM requirements.
About SLN-LOCAL2-RD, RT106S has both commercial grade part and industrial grade part. Thanks!
@Rick_Bye can you help here?
Hi Karina,
Just an FYI, Rick Bye has left NXP, Ming Lin can you provide a contact to address.
Yes, thanks for let me know. I am checking who is the right contact to support this case. As soon as I have the contact, I will reassign this case.