Recommendations for ASR, TTS and Transformer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recommendations for ASR, TTS and Transformer

2,082 Views
QuantumPath
Contributor I

Hello, I am developing an application on i.MX 93 EVK.  I would appreciate recommendations for the following which have relatively low compute requirements while running on-device.  I am using a i.MX 93 Dual core 1.7GHz.

I am looking for recommendations for

  • ASR engine with reasonable accuracy while running on-device.  Eg: Whisper tiny
  • TTS model
  • On-device transformer model such as Llama 3B

    Any information such as performance comparisons and recommendations would be appreciated.  Thank you
0 Kudos
Reply
2 Replies

1,522 Views
Laurent_P
NXP Employee
NXP Employee

Hello  @QuantumPath 

On i.MX93, we have enabled Whisper ASR (tiny, base, small) and Moonshine ASR (tiny and base).

We will deliver first the Whisper ASR as a Voice plugin through GStreamer by mid-July.

For TTS, we have enabled ViTS TTS. For LLM, we can run small LLM like Danube 0.5B.

In parallel, we have a complete eIQ Gen Al flow pipeline (Wake word, ASR, LLM, RAG, TTS) running on  i.MX95 here : https://github.com/nxp-appcodehub/dm-eiq-genai-flow-demonstrator?tab=readme-ov-file

 

372 Views
boopathi12
Contributor I

Hey Laurent_P , can you share how you implemented the Whisper tiny.en TFLite model on the NPU of i.MX93? I’ve been looking for this for ages, and it would really help me in development. I was able to convert the model to TFLite INT8, but the NPU doesn’t fully support all Whisper operations, so I have to use the float32 model on the CPU. Is it even possible to convert it and use it on the NPU?  

thank you 

Tags (1)
0 Kudos
Reply