Is it possible to obtain the file format descriptions for LVVEFS_Rx_Configuration.txt / LVVEFS_Tx_Configuration.txt ?
These configuration files are read by nxp effects libraries liblvvetx.so, liblvverx.so , bundled by Samsung in Android (Marshmellow?)
I have a trace function callback, showing LVVEFS_ArgsReadData
is possibly exitting due to an error ?
03-19 14:09:20.774 3031 3031 W EffectsFactory: T(1): (../SRC/LVVEFS_Create.c:183): FUNCTION: LVVEFS_Create: There are 1 instances of LVVEFS active, id = 73
03-19 14:09:20.774 3031 3031 W EffectsFactory: T(1): (../SRC/LVVEFS_Params.c:131): FUNCTION: LVVEFS_CreateParamTable: LVVEFS_ParseFile starting
03-19 14:09:20.774 3031 3031 W EffectsFactory: T(1): (../SRC/LVVEFS_Parser.c:94): FUNCTION: LVVEFS_ParseFile
03-19 14:09:20.774 3031 3031 W EffectsFactory: T(1): (../SRC/LVVEFS_Args.c:325): FUNCTION: LVVEFS_ArgsReadData
03-19 14:09:20.774 3031 3031 W EffectsFactory: T(1): (../SRC/LVVEFS_Destroy.c:152): FUNCTION: LVVEFS_Destroy: There are 0 instances of LVVEFS active03-19 14:09:20.774 3031 3031 E LvveTxBundle: LVVEFS_Android_Wrapper: Session 73: LVVEFSLibCreate: ERROR while processing returned from LVVEFS_Create 8