missing Qoriva sample code for camera/dc motor/Servo on wiki ?(RESOLVED)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

missing Qoriva sample code for camera/dc motor/Servo on wiki ?(RESOLVED)

2,185 次查看
Grandpierre
Contributor II

Dear Freescale support team,

 

I searched for a while without success the sample Camera code for Qoriva architecture : all the links to the sample code are broken (only the  Blink led sample code is given). For example from this page :

http://thefreescalecup.wikidot.com/qorivva:line-scan-camera
and following ==> Sample Code Download Link <Mail Attachment.gif>Qorivva Sample Code Download Link
==> it returns "The file does not exist."

 

And it is the same for in the "Drive a DC motor tutorial" and "Turning a Servo Tutorial" on Qoriva (It is the same if I sign in or not)

 

Is it normal, does I miss something ?

Thank for your help,

Best regards,

T. Grandpierre

标记 (1)
0 项奖励
回复
1 回复

1,928 次查看
Grandpierre
Contributor II

It's ok : Freescale explained me that the blinking led sample code contain also the others examples

Thank you,

0 项奖励
回复