I have installed the Kinetis Design Studio and KSDK just as your instruction. But when I create a new project and assign the location of KSDK and also select the processor Expert, one error message come to the problem status "There are no supported proces

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I have installed the Kinetis Design Studio and KSDK just as your instruction. But when I create a new project and assign the location of KSDK and also select the processor Expert, one error message come to the problem status "There are no supported proces

跳至解决方案
2,080 次查看
林偉川
Contributor I

I have installed the Kinetis Design Studio and KSDK just as your instruction. But when I create a new project and assign the location of KSDK and also select the processor Expert, one error message come to the problem status "There are no supported processor components found for master processor name "MKL25Z128xxx4_4SDK"". Do I missing something? I just select the processor part as my FRDM-KL25Z. But it seems that the processor expert won't support it?

0 项奖励
回复
1 解答
1,802 次查看
DavidS
NXP Employee
NXP Employee

Hi Wayne,

Please select Processor KL25Z and not Board frdm-kl25z as PE is not supported for the board but does support the Processor.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,803 次查看
DavidS
NXP Employee
NXP Employee

Hi Wayne,

Please select Processor KL25Z and not Board frdm-kl25z as PE is not supported for the board but does support the Processor.

Regards,

David

0 项奖励
回复