Freescale Cup Shield Speed Sensor + KL25Z processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Freescale Cup Shield Speed Sensor + KL25Z processor

3,334 次查看
selvaganesha
Contributor I

Probably a silly question, though I am hopelessly lost.

How does one work the speed sensor on the Freescale Cup shield? Any header files available? Example code?

What i've done so far is connect a hall-effect sensor to the speed sensor port and I can't analyze the data. Though I have verified that it works with the help of an oscilloscope.

While I'm at it, does the Freescale Cup Shield affect the functions of the accelerometer in the KL25Z. Isn't there a standard header file one can download and use?

0 项奖励
回复
5 回复数

2,119 次查看
guillaumeberlan
Contributor I

Hello,

I am also looking for an example.

thank you

0 项奖励
回复

2,119 次查看
admin
Specialist II

Check out these two videos:

Video Link : 1592

Video Link : 1656

2,119 次查看
selvaganesha
Contributor I

These videos give a general idea. Though an example code would be of more use to students.

0 项奖励
回复

2,119 次查看
FlavioStiffan
NXP Employee
NXP Employee

MarekWnuk and RichardBalogh maybe you can help this student as I believe your teams have successfully implemented speed sensors on their cars. Thanks

0 项奖励
回复

2,119 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. University Programs) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 项奖励
回复