ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
Line scan camera data processing - Part I
記事全体を表示
Clip provided by: Hanyang University Korea One of the challenges of the Korea event is to have the cars self-park. This car is using the S12XE chipset.
記事全体を表示
One option for mounting the camera on the Freescale Cup car.  The only additional components you need are two zip ties. [no audio]
記事全体を表示
Find the complete material at:https://community.freescale.com/docs/DOC-95205
記事全体を表示
Find the complete material at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Entrenamiento acerca del LPTMR. Para acceder al material completo visita: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Entrenamiento acerca de NVIC basado en la familia Kinetis L. Para el material completo visita: https://community.freescale.com/docs/DOC-95205
記事全体を表示
Here is a short update via video of the activities done at the University Programs demo area at the Embedded World 2014 Exhibition that was held on 25-27 March 2014 in Nuremberg (Germany).
記事全体を表示
Examine some basic microcontroller concepts, how they are used and some generic I/O paths. The intent is to give the audience a broad picture of microcontrollers and how they are used.
記事全体を表示
In this training video we will examine some concepts in approaching a vehicle control system.  This includes the stages in data flow and update rates of the control software.   The concept of differential steering will be introduced.
記事全体を表示
Continue to explain some common components seen in a microcontroller. Criteria for how a microcontroller is selected will be introduced. View Video Link : 1440
記事全体を表示
In this training video we will decompose an NTSC video signal to gaining understanding of how to capture video data from a "analog" camera.
記事全体を表示
In this training video we will examine some concepts in approaching a vehicle control system.  This includes the stages in data flow and update rates of the control software.   The concept of differential steering will be introduced.
記事全体を表示
Find the complete material at: https://community.freescale.com/docs/DOC-95205
記事全体を表示
EGR280 sophomore design and ECE470/570 Microprocessor based system design at Oakland University (in South East Michigan). Using CW HC12(x) special edition and Wytec Dragon12 dev boards.
記事全体を表示
Illustrates some basic concepts with respect to microcontroller design tools. A generic design flow will be introduced to orient the audience to the most common steps in the software development process.
記事全体を表示
Review the servo example code provided in the FRDM-TFC. TPM peripheral initialization and a simple driver interface will be shown. View Video Link : 1464
記事全体を表示
The Team from the University of Padova in Vicenza are working in getting their race car ready for the upcoming EMEA Finals that will be held in Paris on 26-27 March. They filed this short video on a make up track. Conditions were not the best so they had to scale down the speed.
記事全体を表示
Using Header(.h) files provided by Freescale inside CodeWarrior - Blinking an LED
記事全体を表示
Examines the core used in the MKL25Z128VLK4 device that is mounted on the FRDM-KL25Z board. The audience will be guided through the process of acquiring documentation for both the device and the core. A brief overview of the ARM cortex series will be presentated and how it relates to the embedded systems landscape.
記事全体を表示