Connection Diagram for TRK-MPC560xB to TFC-Shield and TFC-Camera

cancel
Showing results for 
Search instead for 
Did you mean: 

Connection Diagram for TRK-MPC560xB to TFC-Shield and TFC-Camera

No ratings

Connection Diagram for TRK-MPC560xB to TFC-Shield and TFC-Camera

You can view the history of the "motor control shield" here.  The latest Freescale Cup Motor Control board (part number TFC-SHIELD), which is included by default in the kit, is pinned out to directly connect to the FRDM-KL25Z development board.  If you are using the TRK-MPC560xB or other board you will have to direct-wire the connections, as illustrated below.

Labels (1)
Tags (2)
Attachments
Version history
Revision #:
1 of 1
Last update:
‎11-12-2013 12:19 PM
Updated by: