Interfacing the Kinetis board

cancel
Showing results for 
Search instead for 
Did you mean: 

Interfacing the Kinetis board

591 Views
RichardBalogh_n
Contributor II

We just received first cars, unfortunately the kit contains the same interface board as previous year. It is designed to be interfaced with the Quorriva MPC controller board. Do you have any idea how to connect this motor interface to the Kinetis board? Is it possible to obtain different version of the interface for

Kinetis?

0 Kudos
1 Reply

199 Views
FlavioStiffan
NXP Employee
NXP Employee

Richard,

the original cabling and boards were created for MPC5604B board however, the K40 Tower Kit can be used (and has been extensively used) for the Freescale Cup.

Mounting instructions for the board can be found here with examples of cars built with the K40 kit here

There are no wiring instructions as the Tower Kit requires a Proto board (available from me if needed) to make your own connections depending on the configuration you wish to use.

0 Kudos